Meridium Enterprise APM Reliability Analytics offers various tools that help you
analyze the reliability of your equipment and locations so that you can
make decisions about when to repair and replace those pieces of equipment
and locations. For example, a Reliability Distribution Analysis lets you
analyze historical failure data to help predict future failures. Based on those predictions, you can make plans for replacing equipment and
making repairs to prevent future failures. As part of making plans to
replace equipment in the future, you will want to make sure that you have
an adequate number of spare parts available. Having spare parts on hand
will help reduce the amount of downtime associated with unplanned failures.
The key to a successful spares program is maintaining a balance between:
- Optimizing the spares level so that you have enough
spare parts to handle unplanned failures.
- Not having a surplus of parts that are not actually
needed.
You can modify the input data
for a Spares Analysis to evaluate the potential savings or losses associated
with changing the spares level. For example, if you currently keep three
spare seals for a pump, you could use a Spares Analysis to determine whether
it would benefit your company financially to store either more or fewer
spare seals instead.