Access a Reliability Growth Analysis

Steps

  1. Access the RA Overview page.

    Hint: You can also access the RA Overview page for a selected Asset Hierarchy Level.

  2. Select the Reliability Growth tab.

    A list of Reliability Growth Analyses available in the database appears.

    Reliability Growth Section

  3. In the Analysis ID column, select the hyperlink for the analysis that you want to view.

    The Reliability Growth page appears, displaying the Analysis Summary workspace.

    Analysis Summary

    The Analysis Summary workspace contains the Cumulative <Measurement> plot and the MTB<Measurement> plot. These plots are read-only plots. To edit a plot, you must select the corresponding tab from the left pane. The information displayed on this tab will look different depending on the type of data that you use for your analysis.

    The bottom section of the workspace contains the Information and Segments tabs.

    The Information tab displays the following information:

    The Segments tab displays the following columns:

    The left pane in the workspace contains the following tabs:

Copyright © 1993-2016 Meridium, Inc. All rights reserved.