The reliability of an asset or group of assets can be evaluated by subtracting the Probability of Failure from 1 (R = 1-P). The Probability of Failure Plot shows the probability that the unit will survive up to a given age. The Failure Rate plot displays the Failure Rate for a given asset or group of assets based on the System Reliability calculations.
Cumulative Distribution Plot answers the question, "What is the probability of failure by time(t)?" The CDF curve is the area under the PDF curve. The CDF accumulates all probability of failure up to the point in time in question. Since the number of failures increases with increasing time, the slope of the curve is always positive, always increasing.
In addition, you can select one or more Reliability Distribution Analyses from the list of analyses and generate a composite plot to compare the competing failure modes. Competing failure modes occur when the failure pattern, due to one type of fault, dominates the survivor population from another type of fault. If the failure patterns overlap like this, then they are said to be competing failure modes.
Note: If you selected to use a Confidence Level, confidence intervals are included in the analysis calculations and the upper and lower limits appear on the plot.