Calculate the Probability of Failure at a Specified Age

Steps

  1. Access the Reliability Distribution Analysis for which you want to specify the future age to calculate the future probability of failure.
  2. In the left pane, select the Failure Probability tab.

    The Failure Probability information appears in a grid.

    Failure Probability

  3. In the upper-right corner of the grid, select the Distribution Options list, and then select Future Age.

    The Set Future Age window appears. The Future Age field displays the value that was last used to perform the calculation.

    Set Future Age

  4. As needed, enter value in the Future Age box, and then select OK.

    The system recalculates the future probability of failure values and displays them for each piece of equipment in the grid.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.