When viewing the results of a Production Analysis, Production Output is displayed in the Production Data plot and in the Production Loss Regions section. If the data is from a query, the unit of measure is taken into account for production data when the analysis is first created. If the data is from a dataset or manually entered data, then there is no unit of measure associated with the Production Analysis and it has to be set manually. After the analysis exists, you can label the output for the production data with the appropriate unit by setting the unit of measure.
Steps
Access the Production Analysis for which you want to change the unit of measure.
In the left pane, select the Production Data tab.
The Production Data workspace appears.
In the upper-right corner of the workspace, select Analysis Tasks, and then select Unit Of Measure.
The Set Unit Of Measure window appears.
In the Unit Of Measure box, enter the value that characterizes the unit of measure used to collect the data for the Production Analysis, and then select OK.
The Production Analysis is updated. The unit of measure is displayed on the x-axis of the Production Data plot and in the Production Loss Region section on the Quantity column heading. The values in the Quantity column change appropriately.
Copyright © 1993-2016 Meridium, Inc. All rights reserved.