The time units are used for expressing time values for calculations performed within an analysis. For example, a calculation may indicate the amount of time that lapsed between a failure event and the end date of the analysis period. This value would be expressed in the Time Units for the analysis.
Your Time Units selection will depend on what type of data you are using and what type of analysis you are performing. For example, in an analysis that shows the distribution of failures for a number of pieces of equipment or locations over many years, years might be an appropriate unit of time. For an analysis designed to evaluate failures for a single piece of equipment or location within a very specific time period, a smaller unit of time would be appropriate. For this reason, you can choose the Time Units that are most appropriate for a given analysis.
Note: Downtime for TTF calculations should always be provided using days. When the failure data contains downtime, the system selects Days by default.
Steps
Access a Reliability Distribution Analysis for which you want to modify the Time Units.
In the left pane, select the Probability Plot tab.
The Probability Plot appears in the workspace.
Note: You can also modify the analysis period for a plot via the Failure Rate Plot, PDF Plot, CDF Plot, and Failure Probability.
In the upper-right corner of the workspace, select Analysis Tasks, and then select Time Unit.
The Select Time Units window appears.
In the Downtime Unit list, select one of the following options:
Select OK.
The Meridium Enterprise APM system automatically recalculates the analysis based on the new time units and displays the new units on the plots.
Copyright © 1993-2016 Meridium, Inc. All rights reserved.