Create a System Reliability Analysis

To develop a System Reliability Analysis, you must first define the parameters of the analysis, and then create a System Scenario. The analysis parameters serve as inputs to the simulation and will affect the simulation results. You can modify the analysis parameters and rerun the simulation to see the effect that they have on the results.

Steps

  1. Access the RA Overview page.

    Hint: You can also access the RA Overview page for a particular Hierarchy Level.

  2. Select , and then select System Reliability.

    The System Reliability page appears, displaying a blank datasheet in the Analysis Summary workspace.

    Analysis Summary

  3. As needed, enter the values in the available fields, and then select .

    The System Reliability Analysis is created.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.