Create a Reliability Growth Analysis from Manually Entered Data

Steps

  1. Access the RA Overview page.

    Hint: You can also access the RA Overview page for a selected Asset Hierarchy Level.

  2. In the upper-right corner of the page, select , and then select Reliability Growth.

    The Reliability Growth Builder window appears.

    Define New Analysis

    Note: All required information is provided, but for additional information, consult the Reliability Growth and Measurement Data topics.

  3. Enter values in the Analysis Name and Description boxes for the new analysis, and then select Next.

    The Select Data Source Type screen appears. The Data will be based on an existing Query is selected by default.

    Select Data Source Type

  4. Select I will manually enter data, and then select Next.

    The Select Data Format screen appears.

    Select Data Format

  5. On the Select Data Format screen, specify the following:

  6. Select Finish.

    The Reliability Growth Data window appears. The Reliability Growth Data window will look different depending on whether your analysis is using failure dates or cumulative operating time.

    Reliability Growth Data

  7. Enter information about the Failures and Assets that you want to include in the analysis.

    A minimum of three failure datapoints are necessary to perform a calculation.

    Note: If you enter any downtime values that exceed the next failure date, the Meridium Enterprise APM system will highlight the downtime values on the Reliability Growth Data window. The cumulative time between failures will be calculated assuming that the downtime is not accurate and that the failure dates are accurate. When you close the Reliability Growth Data window, an error message will appear. The same error message will also appear in the Analysis Summary workspace.

    Tip: You can add more rows of data by selecting Add at the bottom of the Probability Distribution Data grid . You can remove any row of data by selecting Remove next to the row of data that you want to delete.

  8. Select Finish.

    The Reliability Growth Data window closes. The Meridium Enterprise APM system generates the analysis and the Reliability Growth page appears, displaying the analysis results.

    Analysis Summary

Copyright © 1993-2016 Meridium, Inc. All rights reserved.