Create a Probability Distribution from Manually Entered Data

Steps

  1. Access the RA Overview page.

    Hint: You can also access the RA Overview page for a selected Asset Hierarchy Level.

  2. In the upper-right corner, select , and then select Probability Distribution.

    The Probability Distribution Builder appears, displaying the Define New Analysis screen.

    Define New Analysis

    Note: All required information is provided, but for additional information, consult the Distribution Analysis Families topic.

  3. Enter values in the Analysis Name and Description fields for the new analysis, and then select Next.

    The Select Data Source Type screen appears.

    Select Data Source Type

  4. Select I will manually enter failure data, and then select Next.

    The Select Data Format screen appears.

    Specify Random Variable

  5. In the Random Variable Name box, enter the name of the Random Variable.
  6. In the Units of Random Variable box, enter the units of measure for the Random Variable selected above.
  7. Select Finish.

    The Probability Distribution Data Editor window appears.

    Probability Distribution Data

  8. Enter the information about the random variables that you want to include in the analysis. By default, the following columns are listed on the grid:

    Note: A minimum of three failure data points are needed to perform a calculation or you will receive a warning message and the analysis will not be generated.

    Hint: You can add more rows of data by selecting Add at the bottom of the grid. You can remove any row of data by selecting the Remove next to the row of data that you want to delete.

  1. Select Finish.

    The Meridium Enterprise APM system generates the analysis. The Distribution Data window closes and the Probability Distributionpage appears, displaying the analysis results.

    Analysis Summary

Copyright © 1993-2016 Meridium, Inc. All rights reserved.