Steps
In the left pane, select the Production Data tab.
The Production Data workspace appears.
In the Production Data plot, select the point at which datapoints begin to trend away from the Demonstrated Line.
A dotted line appears and is labeled Process Reliability: <Percentage> , where <Percentage> indicates the reliability of the process.
The following image shows an example of a Process Reliability line showing that reliability of the process is 56.65%:
Copyright © 1993-2016 Meridium, Inc. All rights reserved.