Steps
In the left pane, select the Probability Plot tab.
The Probability Plot appears in the workspace.
Note: You can also modify the value of Random Variable and specify units via the PDF Plot or CDF Plot tabs.
In the upper-right corner of the workspace, select Analysis Task, and then select Change Units.
The Specify the Random Variable window appears.
In the Units box, enter the corresponding units, and then select OK.
The analysis is recalculated using the new Random Variable.
Copyright © 1993-2016 Meridium, Inc. All rights reserved.