TM provides support for a number of handheld data collection devices, referred to within TM as dataloggers. The TM Dataloggers page allows for the collection and transfer of data between TM and a datalogger. This is done by identifying a datalogger in the settings and associating it with one or more mappings, which define the data that is to be sent to and received from the datalogger. TM is shipped with some preconfigured, datalogger-specific mappings. Custom mappings can be added.
Copyright © 1993-2016 Meridium, Inc. All rights reserved.