Before an asset can be accessed via the Thickness Monitoring Overview, you must create Corrosion Analysis Settings for that asset.
Steps
On the top navigation bar, select
The Asset Hierarchy appears.
Below the workspace heading, select the Strategy tab, and then, in the Thickness Monitoring row, select TML Groups.
Note: TML Groups will only appear if you have selected an asset. If you have selected a functional location, Assets replaces TML Groups.
The TM page appears, displaying the Corrosion Analysis Settings workspace.
By default, the Inspection Type box is set to UT. Additionally:
Select Create Settings.
Results
Copyright © 1993-2016 Meridium, Inc. All rights reserved.