About System Codes

System Codes are codes that are defined in a System Code Table. Each table can have an unlimited number of System Codes defined in it. You can manage the codes associated with a System Code Table via the System Codes and Tables page.

In case of a System Code, when you select , the window with System Code name appears, displaying the audit information. On the Create System Code window, this information will not appear as no audit information exists for a new system code.

Copyright © 1993-2017 Meridium, Inc. All rights reserved.