Add References to the System Code

Steps

  1. Access the System Codes and Tables page.
  2. In the System Tables section, select the System Code Table that contains the System Code for which you want to add a reference.

    The properties of the table appears.

  3. In the System Code subsection, select the System Code for which you want to add a reference.

    The References subsection appears.

  4. In the References subsection, select .

    The Add System Code as Reference window appears, displaying the list of references.

    Add System Code as Reference window

  5. Select the reference that you want to add.
  6. Select Add.

    The reference that you have selected is added and appears in the list of references for that System Code in the References subsection.

Copyright © 1993-2017 Meridium, Inc. All rights reserved.