When you create a System Code, a sequence number is assigned for that code. This sequence number defines the order of that System Code relative to other codes in the same System Code Table. If needed, you can modify the sequence order of the System Codes within a given System Code Table.
Steps
In the System Tables section, select the System Code Table that contains the System Codes for which you want to change the sequence.
The properties of the table appear.
In the System Code subsection, select Change Sequence.
The Sequence Change window appears, displaying the list of System Codes.
Modify the order of the System Code by using one of the following methods:
After arranging the System Codes in the required order, select Save.
Your changes are saved, and the System Code section is updated to reflect the new sequence order for the System Code.
Copyright © 1993-2017 Meridium, Inc. All rights reserved.