Create a New Family Field

You can create a new field for a family from scratch, or you can use an existing field as a template for the new field. These instructions provide details on creating a new field from scratch.

Steps

  1. Access the Fields page.
  2. On the Fields page, select .

    The New Field window appears displaying the two section, Information and Behavior.

  3. As needed, enter the values in the available fields in the Information and Field Behavior tabs .
  4. Select Save.

    The new family field is saved and appears in the list on the fields for the family.

Copyright © 1993-2017 Meridium, Inc. All rights reserved.