Delete a System Code Table

Steps

  1. Access the System Codes and Tables page.
  2. In the System Tables section, select the table that you want to delete.

    The properties of the table appear.

  3. In the upper-right corner of the page, select .

    The System Codes and Tables dialog box appears, asking if you want to delete the table.

  4. Select Yes.

    A confirmation message appears, indicating that the System Code Table is deleted.

Copyright © 1993-2017 Meridium, Inc. All rights reserved.