When content validation is enabled, each time a user navigates to Configuration Manager, a check will be performed to ensure that the baseline Meridium Enterprise APM content is valid. If the content is not valid, it will display a warning message. The user will have the option of exporting the invalid content or ignoring the warning.
Steps
Select Enable.
The Meridium Enterprise APM system scans your database for invalid baseline content and displays the results on the Content Summary section in a grid format. Both modifications to and deletions from baseline content are considered invalid and will be included in the list. It displays the following:
Content ID: The ID of the baseline content.
View Name: The property that will be used by Meridium,Inc. for recovering the content.
Type: The type of change occurred on the content. For example, if the baseline content is deleted, it displays the Type as Deletion. If the baseline content is modified, it displays the Type as Modification.
Note: You can disable the content validation on a database on which the content validation is enabled by selecting Disable. The content validation for the baseline content will be disabled and you will no longer receive the warning message in case of a change in the baseline content.
If you want to export the list of invalid contents to an XML file, select Export.
The XML file appears.
Copyright © 1993-2017 Meridium, Inc. All rights reserved.