Import Records and Links

When you import records and links from a legacy format or from a CGU file, the existing relationships in the file will be imported if the predecessor and successor families exist in the database. However, the relationship between the records will not appear in the application.

Steps

  1. Access the Import page.

  2. On the Import page, select Choose File.

    The Open window appears.

  3. Navigate to the folder that contains the CGU file from which you want to import the record, and then select the file.

  4. Select Open.

    The Open window closes, and the file name that you selected appears in the Choose File box. The family IDs and entity IDs of all the records contained in that file appears in the Available Items section listed under Records and Links- CGU .

  5. In the Available Items section:

  6. Select Start Import to import the selected metadata.

    When the import is complete, a confirmation message appears, indicating that the metadata are imported to the database successfully, and a log file in CSV format is generated.

Copyright © 1993-2017 Meridium, Inc. All rights reserved.