Modify the System Code Properties

Steps

  1. Access the System Codes and Tables page.
  2. In the System Tables section, select the System Code Table for which you want to modify the System Codes.

    The properties of the table appear. 

  3. In the System Code subsection, select the System Code that you want to view or modify.
  4. Select .

    A window appears, displaying the details of the System Code.

  5. Modify the System Code properties as required.
  6. Select Save.

    Your changes are saved.

Copyright © 1993-2017 Meridium, Inc. All rights reserved.