Specify Risk Values to Determine an Overall Risk Rank

You can use the Risk Assessment window to select values in various categories that will be used to determine an overall risk rank.

Note: These steps assume that you want to specify a risk value on each tab of the Risk Matrix. You can, however, specify that a risk category does not apply to the current risk.

Steps

  1. In GE Digital APM, access the Risk Assessment window.

    Hint: Refer to a specific module's documentation for details on how to access this window.

  2. On each tab that contains a risk matrix, select the cell whose value represents the risk for that category.

    An icon appears in the selected cell. The way in which you accessed the Risk Assessment window determines the icon that appears in the cell.

    Note: When defining mitigated risk, you cannot select a value with a higher probability or consequence than the value that is already represented by the icon. For example, suppose the icon appears in the cell at the intersection of the Probable probability (1) and Low consequence (10). In this case, using the icon, you could not select a value with a probability greater than 1 or a consequence greater than 10.

  3. Select the Financial tab, if applicable.
  4. In each list or box on the Financial tab, select or enter the necessary value.

    The values that you type in the Production Loss and Maintenance Cost boxes will be added together to determine the overall consequence, which is displayed in the Consequence box.

    Note: If you are defining mitigated risk, the mitigated financial values must be lower than the unmitigated financial values.

  5. Select Save.

Results

Copyright © 2017 General Electric Company. All rights reserved.