Passive IPL records store information about the probability of failure of various types of passive IPLs. This topic provides an alphabetical list and description of the fields that exist for the Passive IPL family. The information in the table reflects the baseline state and behavior of these fields.
IMPORTANT: The records in this family can be modified only by users who belong to the Security Groups MI SIS Administrator or MI HA Administrator.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
|
Field |
Data Type |
Description |
Behavior and Usage |
|---|---|---|---|
|
Default Value |
Numeric |
Indicates the default probability that the Passive IPL will fail to mitigate the risk. |
You can enter a value manually. |
| Lower Range | Numeric | Indicates the lower range for the probability that the Passive IPL will fail to mitigate the risk. |
You can enter a value manually. |
| Passive IPL ID | Character | Identifies the type of Passive IPL. |
This field appears a list that is populated by the MI_PASSIVE_IPL System Code Table. |
| Upper Range | Numeric | Indicates the upper range for the probability that the Passive IPL will fail to mitigate the risk. |
You can enter a value manually. |
Copyright © 2017 General Electric Company. All rights reserved.