Suppose that in your facility, you have two tanks that
are connected with a pipe or a piping system, where hazardous chemicals in one tank are transferred
to the other tank through the pipe or the piping system. The continual process of monitoring
the liquid level in each tank, increasing or decreasing it as needed, and
transporting the chemicals from the source tank to the target tank is
a potentially hazardous process that involves risk. During this process,
for example, if the level control malfunctions, the pressure in the
pipe or the source tank could increase too rapidly and cause the chemicals in the source
tank to leak out, causing damage to the environment or personnel.
After you identify the hazardous scenarios associated with a process,
you can use Hazards Analysis to:
- Define the characteristics of the scenarios, including
the risks that they include.
- Assess the likelihood of the risks in each scenario
actually occurring.
- Identify ways to prevent the risk in each scenario
from occurring.
- Make recommendations for actions that can be taken
within the facility to prevent the risks in each scenario from occurring
or to mitigate the risks in some way (e.g., lower the severity of
the safety or environmental impact).
Suppose that, for the preceding process (transporting hazardous
chemicals between two tanks), you identify a risk that the pressure monitor
will stop working and a chemical spill will occur. Through a risk assessment,
you also determine that the chemical spill is very likely to cause a negative
impact to both human safety and the environment. Based on this assessment,
you might determine that the only way to prevent the risk is to be alerted
when the pressure in the tank is increasing too quickly. In this case,
you may recommend that a high pressure alarm be put in place to alert someone
if the pressure in the tank is rising too quickly. You may recommend to test the alarm on a periodic basis to ensure the availability of the alarm.