Add Inspection Confidence Evaluations

Steps

  1. Access the Inspection Data section.
  2. In the workspace heading, select the Inspection Confidence Evaluation tab.

    The Inspection Confidence Evaluation section appears.

  3. In the Inspection Confidence Evaluation section, as needed, enter values in the available fields. All required information is provided, but for additional information, refer to the Inspection Records topic.

    IMPORTANT: The Inspection Confidence Evaluation tab will be disabled for both PRD Pop Test Checklists and External PRD Checklists. For those checklists, to modify the following fields, edit the values in the Inspection Data section.
    1. In the Degradation Mechanism field, select the degradation mechanism that you want to add to the Inspection Confidence Evaluation.

    2. In the Type of Inspection field, select the inspection type that you want to add to the Inspection Confidence Evaluation.

    3. In the Extent field, select the extent that you want to add to the Inspection Confidence Evaluation.

      Note: The Scope field populates automatically based on the information provided in the Extent field.

  1. Select .

    A new Inspection Confidence Evaluation is added to the selected inspection, and a new row appears.

    Tip: As needed, you can repeat steps 3 and 4 to add multiple Degradation Mechanisms to the selected Inspection Confidence Evaluation.

Result

Copyright © 2017 General Electric Company. All rights reserved.