Unmitigated Consequence Frequency = Frequency of Initiating Event x Probability of occurrence of Enabling Event x Probability of occurrence of Conditional Modifier
Where,
If Enabling Event/Condition Probability field is blank, a default value of 1 will be used in the calculation.
Total IPL PFD = Product of value in PFD field of all the Safeguards associated with the LOPA
Mitigated Consequence Frequency = Unmitigated Consequence Frequency x Total IPL PFD
Where,
If there are no IPLs associated with the LOPA, then Mitigated Consequence Frequency is equal to the Unmitigated Consequence Frequency.
Required PIF PFD = Required Mitigated Consequence Frequency / Mitigated Consequence Frequency
Where,
Required PIF Risk Reduction Factor = 1/ Required PIF PFD
Where,
This value is derived based on the industry standard for SIL values.
The following table contains the data used in the example and only lists fields that are required and contain a value.
Field | Value |
---|---|
Suppose that you create a LOPA with the following values: |
|
LOPA ID | Lopa_Example |
Unacceptable Consequence | Explosion |
Initiating Event Type | Gasket/packing blowout |
Frequency of Initiating Event | 0.01 |
Required Mitigated Consequence Frequency | 1E-05 (i.e., 0.00001) |
Fields that are automatically populated in LOPA | |
Unmitigated Consequence Frequency | 0.01 |
Mitigated Consequence Frequency | 0.01 |
Required PIF Risk Reduction Factor | 1000 |
Required PIF PFD | 0.001 |
Calculated SIL | 2 |
Create a Conditional Modifier with the following values: | |
Conditional Modifier ID | Modifier1 |
Type | Probability of Ignition |
Probability | 0.5 |
Fields that are updated in LOPA after adding a Conditional Modifier | |
Unmitigated Consequence Frequency | 0.005 |
Mitigated Consequence Frequency | 0.005 |
Required PIF PFD | 0.002 |
Required PIF Risk Reduction Factor | 500 |
Calculated SIL | 2 |
Create a Safeguard and specify as IPL with the following values: | |
Safeguard ID | Safeguard1 |
IPL Type | Human IPL |
IPL Sub Type | Human Action with >10 min response time |
PFD | 0.1 |
Fields that are updated in LOPA after adding a Safeguard that is an IPL | |
Total IPL PFD | 0.1 |
Unmitigated Consequence Frequency | 0.005 |
Mitigated Consequence Frequency | 0.0005 |
Required PIF PFD | 0.02 |
Required PIF Risk Reduction Factor | 50 |
Calculated SIL | 1 |
Copyright © 2017 General Electric Company. All rights reserved.