This topic describes how to change the state of a LOPA, while assigning the state of the LOPA to the appropriate user.
IMPORTANT: You can modify the state for a LOPA only if you are an administrator or a user who belongs to the State Configuration Role configured for that state.
Results
If you changed the state of LOPA linked to a LOPA Assessment of an Instrumented Function in a SIL Analysis to Complete, then the values in the associated LOPA Assessment and Risk Assessment are updated based on the values in the LOPA. If linked to a LOPA Assessment of an Instrumented Function in a SIL Analysis, the following records are also updated:
Copyright © 2017 General Electric Company. All rights reserved.