Add a Risk Threshold

Steps

  1. Access the Risk Threshold records associated with a Risk Matrix.
  2. In the Record Explorer pane, in the Risk Threshold heading, select .

    An option menu appears.

  3. If a Risk Threshold record already exists for the consequence you want to associate with the Risk Matrix:

    1. Select Link Existing Record.

      The Search window appears.

    2. Enter search criteria to locate the record that you want to associate with the Risk Matrix.
    3. Select the record, and then select OK.

    -or-

    If a Risk Threshold record does not already exist for the consequence you want to associate with the Risk Matrix:

    1. Select Add New Record.

      A blank datasheet for the new Risk Threshold appears.

    2. In the Alias box, , if the Use Aliases? check box is selected in the associated Risk Matrix record, specify a value that you want to appear on the Risk Matrix in the column heading along with the consequence name.
    3. In the Description box, select from the drop-down menu.

      Note: The values that you can select in a new Risk Threshold record are determined by the MI_RISK_THRESHOLD System Code Table.

    4. In the Value box, enter the value that you want to correspond to the risk threshold.
    5. In the Color field, select the color that you want to set for this risk threshold.
    6. Select .

    Your changes are saved and can be viewed in the matrix on the Risk Matrix Preview window.

Copyright © 2017 General Electric Company. All rights reserved.