Configure Email Settings (SMTP)

Note: You can either configure the SMTP server or use the IIS Drop Folder.

Steps

  1. Access the Email Settings page.
  2. On the Email Settings page, in the SMTP Host box, enter the unique name of your SMTP server.

    Note: You can enter LocalHost in the SMTP Host box. Setting the name to LocalHost indicates the use of an SMTP server on the local computer. Typically, it is the default SMTP server.

  3. In the From box, enter the email address that you want to appear in the From field of emails generated by GE Digital APM.
  4. Select .

    All the emails are now configured to be sent via the SMTP server.

    Tip: To send a test email to confirm that email settings have been configured successfully, select Test Settings, then, on the window that appears, enter values in the available fields, and then select Send.

Copyright © 2017 General Electric Company. All rights reserved.