Steps
Server Name: Enter the name of the server on which the desired instance of SQL Server Reporting Services has been installed and configured.
Note: If you do not specify the protocol for the server, HTTP will be assumed. If the SQL Server Report Server is a secured server, you can type HTTPS://[Server Name] to indicate that an HTTPS connection should be used. If the SQL Server Report Server is not secured, you can type HTTP://[Server Name] or you can omit the protocol and simply type the server name.
Web Service: Enter the name of the Report Server Virtual Directory that has been created for the instance of SQL Server Reporting Services that you want to use for the current GE Digital APM Server and data source.
If you have never before defined the SQL Server Report Server for this data source, the Web Service will be set to Report Server by default, which is the name of the virtual directory created for the first SQL Server Report Server instance that is installed on a given server. You can modify the default value if needed.
If the server specified in the Report Server text box contains multiple instances of SQL Server Reporting Services, be sure to specify the virtual directory of the instance that you want to use for the GE Digital APM Server and data source to which you are currently connected.
Copyright © 2017 General Electric Company. All rights reserved.