Modify the Asset Hierarchy Configuration

Note: You only need to modify the Asset Hierarchy if you want to change the baseline configuration.

Steps

  1. Access the Asset Hierarchy Configuration page.
  2. For the section you want to use as the primary level of the hierarchy, select Root.

  3. In the Root section, select a value for the following as necessary:

  4. If you want to add another level, in the upper left corner of the page, select , and then configure the values as needed.
  5. To save, but not apply, the modifications, select .

    -or-

    To apply the modifications, select , and then select Rebuild.

    The modifications are applied, and are reflected on the Assets page.

Copyright © 2017 General Electric Company. All rights reserved.