Create a GE Connection Record

You can use the GE Connection section of the GE Connection workspace to create a GE Connection record.

Note: There can only be one GE Connection per GE Digital APM System.

Steps

  1. On the Connections page, access the GE Connection section.

  2. In the Connection subsection, populate the following fields on the GE Connection record.

  3. To use an SSL Connection, select the Use SSL check box, and then complete the following SSL configuration fields on the GE Connection record.

  4. Select .

    The GE Connection record is created.

Results

Copyright © 2017 General Electric Company. All rights reserved.