Modify the Risk Assessment Window Title

You can modify the default title of the Risk Assessment window using the Risk Matrix record.

Note: When you modify the title, the new title will be used everywhere that the Risk Matrix record is used to display the Risk Assessment window. For example, if an Asset Strategy and an RCM Analysis use the same Risk Matrix, if you modify the title in that Risk Matrix record, the new title will be displayed when you access the Risk Assessment interface from any of the following items:

Steps

  1. Access the Risk Matrix record for the Risk Matrix that you want to modify.
  2. On the Risk Matrix Layout datasheet, select .
  3. In the Appearance section, in the Dialog Title box, enter the new title for the Risk Assessment window.

    Note: The default title is not displayed on the datasheet. If the Dialog Title text box is empty, it indicates that the default title is being used.

  4. Select .

    Your changes are saved. The next time you view the Risk Assessment window from any item that uses this Risk Matrix (e.g., an Asset Strategy or RCM Analysis), the new title will appear.

Copyright © 2017 General Electric Company. All rights reserved.