Risk Matrix Records

Risk Matrix records determine how a Risk Matrix looks, as well as other information about the Risk Matrix. This topic provides an alphabetical list and description of the fields that exist for the Risk Matrix family and appear on the Risk Matrix Layout datasheet. The information in the table reflects the baseline state and behavior of these fields.

Field

Data Type

Description

Behavior and Usage

Alias Format Mask

Character

Specifies the format in which you want to display the risk rank values in the cells on the risk matrix.

The format must be defined using the following formula:

{c} - {r} - {pl} - {t}

Where:

  • {c} is the alias for the column.
  • {r} is the alias for the row.
  • {pl} is the alias for the protection level.
  • {t} is the alias for the risk threshold.

The delimiter in this formula is a dash (-), but it can be customized. For example, if desired, you could use a colon (:), in place of a dash.

You can exclude from the format any parameter that you do not want to see on the risk matrix.

The default format is {c} - {r}.

Consequence Axis

Character

Specifies the axis on which the consequence values are displayed.

You can choose from:

  • X-Axis: Displays the consequence values along the x-axis.
  • Y-Axis: Displays the consequence values along the y-axis.

When you change this value, the value in the Probability Axis field is updated automatically to display the opposite value.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, the default value is X-Axis.

Consequence Sort Order

Character

Specifies the order in which the consequence values are displayed.

You can choose from:

  • Ascending: Displays the consequence values in ascending order.
  • Descending: Displays the consequence values in descending order.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, the default value is Ascending.

Currency

Character

Specifies the unit of measure that appears next to the Consequence box on the Financial tab of the Risk Matrix.

After the Risk Matrix has been used by a module in GE Digital APM, this field is disabled, and you cannot modify the value.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, the default value is USD.

Default

Boolean

Indicates whether or not this Risk Matrix is the default Risk Matrix.

You can specify only one Risk Matrix record as the default. If you specify a second Risk Matrix record as the default, a message will appear, indicating that you must first clear the Default check box on the Risk Matrix record that is currently set as the default before you can specify a different Risk Matrix as the default.

In the Standard Practice Risk Matrix record, the Default check box is cleared. In the Default Risk Matrix record, the Default check box is selected.

Dialog Title

Character

Specifies the title of the Risk Assessment window that appears when accessed from an item that uses this Risk Matrix (e.g., an Action in an Asset Strategy).

In the baseline Risk Matrix record and all new Risk Matrix records that you create, the Dialog title box is empty, indicating that the default title is being used.

Hide Numeric Risk Rank?

Boolean

Indicates whether or not you want to display the numeric risk rank values in the Risk Matrix.

If this check box is cleared, the numeric risk rank values are displayed. If this check box is selected, the numeric risk rank values are hidden in the Risk Matrix.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, this check box is cleared.

Hide Probability and Consequence Names

Boolean

Indicates whether or not the Probability and Consequence names are hidden on the Risk Matrix.

If the check box is cleared, the names are displayed. If the check box is selected, the names are hidden.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, this check box is cleared.

Hide Protection Level Text

Boolean

Hide Protection Level Text.

This allows the user to hide the text boxes that normally show the unmitigated and mitigated protection level values in the Risk Assessment window.

Lock Mitigated Consequence

Boolean

Indicates whether or not the mitigated consequence is locked.

When this check box is selected, for mitigated risk assessments, you will be able to modify only the probability value. You will not be able to modify the consequence value.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, the check box is selected.

Logarithmic Scale

Boolean

Indicates whether or not the y-axis will use a logarithmic scale on a graph that displays risk values.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, this check box is selected.

Mitigated Risk Rank

Character

Specifies the label of the Risk Assessment window section that displays the mitigated risk rank.

The default label is Mitigated Risk Rank.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, the Mitigated Risk Rank box is empty, indicating that the default title is being used.

Mitigation Label

Character

Specifies the label of the Risk Assessment window section that displays the name of the item that is mitigating the risk.

The default label is Mitigated By.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, the Mitigation Label box is empty, indicating that the default title is being used.

Probability Axis

Character

Specifies the axis on which the probability values are displayed.

You can choose from:

  • X-Axis: Displays the probability values along the x-axis.
  • Y-Axis: Displays the probability values along the y-axis.

If you change this value, the value in the Consequence Axis field will be updated automatically to display the opposite value.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, the default value is Y-Axis.

Probability Sort Order

Character

Specifies the order in which the probability values are displayed.

You can choose from:

  • Ascending: Displays the probability values in ascending order.
  • Descending: Displays the probability values in descending order.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, the default value is Descending.

Risk Matrix Name

Character

The name of the Risk Matrix.

This value is used to identify the record. It does not, however, appear anywhere on the Risk Assessment interface.

In the baseline Risk Matrix record, the Risk Matrix name is Default.

If you copy a Risk Matrix, the value in the Risk Matrix Name field in the new Risk Matrix record will be set to Copy of <Name>, where <Name> is the name of the Risk Matrix record that you copied. After you create a copy of a Risk Matrix, you can modify it as desired.

Show Financial Impact Boolean Indicates whether or not the Financial Impact field of the Risk Rank family appears on each category tab the Risk Matrix.

This field appears on the Risk Matrix Layout and the Risk Matrix Definition datasheets.

If the Show Financial Impact check box is cleared, the Financial Impact value does not appear on each category section of the Risk Matrix. If the Show Financial Impact check box is selected, then the Financial Impact value appears on each category section of the Risk Matrix.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, this check box is cleared by default.

Unmitigated Risk Label

Character

Specifies the label of the Risk Assessment window section that displays the name of the risk.

The default label is Risk Of.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, the Unmitigated Risk Label box is empty, indicating that the default label is being used.

Unmitigated Risk Rank

Character

Specifies the label of the Risk Assessment window section that displays the unmitigated risk rank.

Note: If you are using the Asset Criticality Analysis feature, this value will also be used as the label of the column that displays the unmitigated risk rank in ACA.

The default label is Unmitigated Risk Rank.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, the Unmitigated Risk Rank box is empty, indicating that the default label is being used.

Use Aliases?

Boolean

Indicates whether or not you want to display the aliases that have been defined for the records that are linked to the Risk Matrix record. For example, if the Alias field in the Consequence record High contains the value E , when the Use Aliases? check box is selected, instead of seeing only the value High in the Risk Matrix, the value E will appear.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, this check box is disabled and cleared. It becomes enabled only when you select the Use Maximum Risk Rank check box.

Use Maximum Risk Rank

Boolean

Indicates whether or not the overall risk rank will equal the largest value of all selected values (except for the Financial value) in Risk Matrix.

If this check box is cleared, the overall risk rank will equal the sum of all selected values (except for the Financial value).

After the Risk Matrix has been used by a module in GE Digital APM, this field is disabled, and you cannot modify the selection.

In the baseline Risk Matrix record and all new Risk Matrix records that you create, this check box is cleared.

Copyright © 2017 General Electric Company. All rights reserved.