Schedule Work Orders

Steps

  1. Access the APM Connect page.

    The APM Connect Configuration page appears.

  2. Select EAM Settings.

    The EAM Settings page appears.

  3. In the Scheduling Properties section, select Edit Schedule.

    Note: If there is a previously schedule item, a schedule summary will be displayed next to Edit Schedule. If there is no scheduled item, Not scheduled appears next to the Edit Schedule button.

  4. On the Edit Schedule window, select the Recurrence check box.
  5. In the Time Zone box, select the appropriate time zone.
  6. In the Start box, select to schedule the start date and time.

    1. Select one of the following as appropriate:

      • The current date: Select this option to use the current time and date as the starting point.
      • Clear: Select this option to clear the current selection.
      • <Date>: Select this option to use the selected date as the start date.
    2. Select , and then select the appropriate time.
    3. Select Close.
  7. In the Every section, in the interval box, enter the numeric value for how often you want the generation to occur.
  8. In the Every section, in the units box, select the interval unit (i.e., minutes, hours, years, etc).
  9. In the Every section, in the begin box, select one of the following:

  10. In the End box, based on when you want the recurrence to end, use the drop-down to select one of the following:

  11. Select OK.

    The schedule summary appears next to the Edit Schedule. Additionally, the scheduled item can be viewed in Operations Manager in Scheduling.

Copyright © 2017 General Electric Company. All rights reserved.