The following diagram shows how the families used in RCM are related to one another.
Note: In the diagram, boxes represent entity families and arrows represent relationship families that are configured in the baseline database. You can determine the direction of the each relationship definition from the direction of the arrow head: the box from which the arrow originates is the predecessor, and the box to which the arrow head points is the successor.
In the preceding diagram:
The RCM FMEA Asset box represents a single RCM FMEA Asset record within an analysis. The RCM FMEA Analysis record can be linked to multiple RCM FMEA Asset records, each of which can be linked to an Equipment or Functional Location record.
The Equipment or Functional Location box represents the Equipment or Functional Location family for which the Is RCM FMEA Asset, Has Recommendations, and Has Tasks have been defined between that family and the specified predecessor or successor.
When an RCM FMEA Recommendation record is created for the analysis, the Recommendation record is linked to the Equipment or Functional Location record to which the RCM FMEA Asset record is linked.
When an RCM FMEA Recommendation record is promoted to an Action record, the Action record will be linked to a Proposed Strategy record and associated with the Equipment or Functional Location record. For details, see the ASM Help.
The following table provides a summary of the entity families and relationship families that are used to develop an RCM Analysis.
Records in this entity family:
...Can be linked to records in this entity family:
...Through a relationship definition on this relationship family:
RCM FMEA Analysis
RCM Function
Has RCM Function
RCM Function
RCM Functional Failure
Has RCM Functional Failure
RCM Functional Failure
RCM FMEA Failure Mode
Has RCM FMEA Failure Mode
RCM FMEA Failure Mode
RCM FMEA Failure Effect
Has RCM FMEA Failure Effect
RCM FMEA Failure Effect
RCM FMEA Recommendation
Has RCM FMEA Recommendation
In addition, the following families and relationships are used by RCM by not within the analysis tree itself.
Records in this entity family:
...Can be linked to records in this entity family:
...Through this relationship:
Purpose
RCM FMEA Analysis
Human Resource
Has RCM FMEA Team Member
Facilitates the construction of the RCM Analysis Team Members list. Through this relationship, Human Resource records are linked directly to the RCM FMEA Analysis record.
RCM FMEA Analysis
RCM FMEA Asset
Has RCM FMEA Asset
Facilitates the construction of the RCM equipment list. In this way, the RCM FMEA Asset records are linked directly to the RCM FMEA Analysis record. Note, however, that RCM FMEA Asset records do not appear in the analysis tree of an RCM Analysis.
RCM FMEA Analysis
RCM FMEA Task
Has Tasks
Allows Task records generated from Recommendation records to be linked to the RCM FMEA Analysis record for which the recommendation was created. Note that in the current version of GE Digital APM, RCM FMEA Task records cannot be created from RCM FMEA Recommendation records. Instead, RCM FMEA Recommendation records can be used to create Action records in ASM. This relationship still exists, however, to support legacy RCM FMEA Task records.
RCM FMEA Recommendation
RCM FMEA Task
Has Tasks
Allows RCM FMEA Recommendation records to be linked to RCM FMEA Task records that are generated from those recommendations. Note that in the current version of GE Digital APM, RCM FMEA Task records cannot be created from RCM FMEA Recommendation records. Instead, RCM FMEA Recommendation records can be used to create Action records in ASM. This relationship still exists, however, to support legacy RCM FMEA Task records.
RCM FMEA Asset
Asset Strategy Template
Has Strategy
Facilitates the promotion of RCM FMEA Asset records to Asset Strategy records via Recommendation Management. This link is established when an RCM FMEA Analysis is linked to a physical or "virtual" piece of equipment or location for which you have defined Recommendation records.
RCM FMEA Asset
RCM FMEA Task
Has Tasks
Allows RCM FMEA Asset records to be linked to RCM FMEA Task records. This link is established only when a Task record is generated from a recommendation where the related RCM FMEA Asset record (i.e., the RCM FMEA Asset record that is linked to the RCM FMEA Analysis record) is not linked to an Equipment or Functional Location record.
Note that in the current version of GE Digital APM, RCM FMEA Task records cannot be created from RCM FMEA Recommendation records. Instead, RCM FMEA Recommendation records can be used to create Action records in ASM. This relationship still exists, however, to support legacy RCM FMEA Task records.
RCM FMEA Asset
Task History
Has Task History
Facilitates the rejection of RCM FMEA Task records that are linked to RCM FMEA Asset records. When you reject an RCM FMEA Task record, a Task History record is created and linked to the RCM FMEA Asset record through the Has Task History relationship.
RCM FMEA Asset
Task History
Has Task History
Facilitates the rejection of RCM FMEA Task records that are linked to RCM FMEA Asset records. When you reject an RCM FMEA Task record, a Task History record is created and linked to the RCM FMEA Asset record through the Has Task History relationship.
RCM FMEA Analysis
RCM FMEA Template
Has Templates
Facilitates the creation of RCM Templates.
RCM FMEA Asset
RCM FMEA Template
Has Templates
Facilitates the creation of RCM Templates.
RCM Function
RCM FMEA Template
Has Templates
Facilitates the creation of RCM Templates.
RCM Functional Failure
RCM FMEA Template
Has Templates
Facilitates the creation of RCM Templates.
RCM FMEA Failure Mode
RCM FMEA Template
Has Templates
Facilitates the creation of RCM Templates.
RCM FMEA Recommendation
Mitigates Risk
Risk Assessment
Allows you to determine how a recommendation mitigates a risk.