This topic provides an alphabetical list and description of the fields that exist for the RCM FMEA Template family and appear on its datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
|
Field |
Data Type |
Description |
Behavior and Usage |
|---|---|---|---|
| Analysis Type | List | The type of analysis the template is based on. | This field is populated automatically with RCM and cannot be modified. |
| Approved Date | Date/Time | The date on which the template was approved. | You can use the Calendar feature to select the date on which the template was approved. |
| Approver | Character | The person who approved the template. | Enter the name and/or title of the approver. |
| Author | List | The user that created the template. | This field is generated automatically and cannot be modified. |
| Created On | Date/Time | The date on which the template was created. | This field is generated automatically and cannot be modified. |
| Criticality | Character | The degree to which an asset is functionally or economically important. | This field is read-only and populated automatically. |
| Description | Text | Details for the template. | You can enter a description manually. |
| Duty | Character | The duty cycle context under which the asset is operating (i.e., continuous or standby). | This field is read-only and the value is populated by the APT template data load. |
|
ID |
Character |
The ID of the template. |
This is a required field. It can be modified, but each template ID must remain unique. |
| Service | Character | The process and environmental conditions under which the asset is operating. | This field is read-only and the value is populated by the APT template data load. |
| Status | List | The status of the template. |
This field will contain on of the following values:
|
| Template Category | Character | Any category name you want to assign to the template. | Enter a category in the field. |
| Template Notes | Text | Any additional information you want to provide about the analysis template. | Enter additional notes in the field. |
| Type | Text | The family of the record from which the template was created. | This field is generated automatically and cannot be modified. |
Copyright © 2017 General Electric Company. All rights reserved.