Create an RBI Corrosion Loop

This topic describes how to create a Corrosion Loop and link it to a Process Unit. You can also link an existing Corrosion Loop to a Process Unit.

Steps

  1. Access the Process Unit for which you want to create a Corrosion Loop.
  2. In the left pane, select , and then select Create New Corrosion Loop.

    The Corrosion Loops Details section appears, displaying a blank datasheet for the Corrosion Loop. The value in the RBI Corrosion Loop ID field is populated automatically.

  3. As needed, enter values in the available fields.
  4. In the upper-right corner of the section, select .

    The RBI Corrosion Loop is created, and linked to the selected Process Unit.

What's Next?

Copyright © 2017 General Electric Company. All rights reserved.