Create an RBI Component

This topic describes how to create a new RBI Component and link it to an Asset or a Corrosion Loop. You can also link an existing RBI Component to an Asset or a Corrosion Loop.

Steps

  1. Access the Asset Summary workspace of the asset in which you want to create an RBI Component.

    -or-

  2. Access the Corrosion Loop in which you want to create an RBI Component.
  3. In the left pane, select , and then select Create New Component.

    The Create New RBI Component window appears.

  4. Enter values in the following fields:

  5. Select Create.

    A new RBI Component is created, and is automatically linked to the selected Asset and the Corrosion Loop. The Component Details section appears, displaying the component datasheet.

  6. Enter values in the available fields.
  7. In the upper-right corner of the datasheet, select .

    The changes made to the RBI Component are saved.

Results

What's Next?

Copyright © 2017 General Electric Company. All rights reserved.