This topic describes how to add a Failure Mode node to the Logic Tree from the design canvas. You can also copy an existing Failure Mode node, import an existing RCA Failure Mode node, or import a failure mode from FMEA and RCM.
Steps
In the upper portion of the workspace, in the Palette section,
select , and then use the drag-and-drop method to add the icon to the Failure Event
node in the design canvas.
The Properties window appears, displaying the datasheet for the selected Failure Mode node.
Select
The RCA Failure Mode node is saved and automatically linked to the RCA Event and the RCA.
What's Next?
Copyright © 2017 General Electric Company. All rights reserved.