RCA Hypothesis Records

RCA Hypothesis records store basic information about root cause of a failure event. The following table provides an alphabetical list and description of the fields that exist for the RCA Hypothesis family and appear by default on the RCA Hypothesis datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field Caption Data Type Description Behavior and Usage
Confidence Factor Character A value that indicates the probability that the hypothesis is true.

You can choose from the following values:

  • Not True (0)
  • Somewhat true (1)
  • Possibly True (2)
  • Likely (3)
  • Highly Likely (4)
  • True (5)

If you select a value in this field, the value that you select will appear in brackets to the right of the hypothesis name in the Logic Tree.

Description Text A detailed description of the hypothesis.

You can define this value manually when you create the RCA Hypothesis.

ID Character The ID for the Hypothesis.

This field is automatically populated and is disabled.

Label

Character A description of the hypothesis as you want it to appear on the Logic Tree.

You can define this value manually when you create the RCA Hypothesis.

State Character The state of the Hypothesis node.

You can choose from the following states:

  • Hypothesis
  • Hypothesis True
  • Hypothesis Not True
  • Cause Human
  • Cause Latent
  • Cause Physical

This field is set to Hypothesis by default.

Copyright © 2017 General Electric Company. All rights reserved.