Send a Summary of Findings Via Email

After the RCA Team has successfully identified the root causes associated with the failure that was investigated, the next step involves communicating the team's findings and proposing recommendations to the appropriate individuals within your organization. To do so, you can:

Steps

  1. Access the Root Cause Analysis for which you want to communicate the findings.
  2. In the left pane, select the Communicate Findings tab.

    The Communicate Findings workspace appears. The Comprehensive Analysis Report tab is selected by default, displaying the Comprehensive Analysis Report section.

    Communicate Findings

  3. Select to add one or more users to whom you want to send the Comprehensive Analysis Report.

    The Add Users section appears, displaying the list of human resources in the left section.

    Add Users

  4. In the left side of the section, select the Human Resource record, and then select .

    The user represented by the Human Resource record is added to the right side of the section.

    Hint: You can add more than one user.

  5. Select to go back to the Comprehensive Analysis Report section.
  6. In the RCA Communicate datasheet, modify the values in the available fields as needed.

  7. In the upper-right corner of the workspace, select Send.

    The Comprehensive Analysis Report is sent to the selected user via an email. The email contains the Comprehensive Analysis Report as an attachment as well as the following information:

    Comprehensive Analysis Report

What's Next?

Copyright © 2017 General Electric Company. All rights reserved.