Specify a Default Home Dashboard

You can specify the dashboard that will appear on the home page by default when a new user logs in to GE Digital APM.

Note: If you do not specify a default dashboard, the GE Digital APM dashboard will appear. This dashboard is stored in the following Catalog location: //Public/Meridium/Modules/Core/Dashboards/APM Foundation Dashboard

Steps

  1. Access the User Defaults page.
  2. In the Default Home Dashboard box, select .

    The Select a dashboard from the catalog window appears.

  3. Navigate through the Catalog, and then select the Dashboard that you want to set as the default dashboard.

  4. Select Open.

    The default dashboard is specified.

Copyright © 2017 General Electric Company. All rights reserved.