Create a Data Source

Steps

  1. Access the Data Sources page.
  2. In the upper right corner of the page, select .

    An empty Data Source form appears.

  3. In the Data Source ID box, enter a name for the data source.

    IMPORTANT:

    • This value is required, and must be unique for the GE Digital APM Server.
    • This value cannot contain spaces or any special characters; it should be alphanumeric.
    • This value cannot be modified after you save the data source.
  4. In the Data Source Description box, enter a description of the data source.

    Note: The description of the data source will be displayed on the GE Digital APM Welcome page, in the list of available data sources.
  5. In the Data Source Host box, if you are a GE Digital APM Now customer, enter the host name or address. Otherwise, the value in this box should be *.
  6. In the Database Type list, select either Oracle or SQL Server.

    If you selected Oracle, the following boxes are enabled:

    If you selected SQL Server, the following boxes are enabled:

  7. If you selected Oracle in step 6, then either enter a value in the Database Alias box, or enter values in the Oracle Host, Oracle Port, and Oracle Service boxes.

    Note: A database alias, contained within a tnsnames.ora file, contains the Oracle host, port, and service information related to the database, and may have been set up by a database administrator to simplify access. To determine whether a database alias has been created, and to determine the appropriate values for the Database Alias box or Oracle Host, Oracle Port, and Oracle Service boxes, contact your database administrator.

    If you selected Oracle in step 6, then you do not need to enter values in the Database Server and Database Name boxes.

    -or-

    If you selected SQL Server in step 6, then enter values in the Database Server and Database Name boxes.

    Note: If you selected SQL Server in step 6, then you do not need to enter values in the Database Alias, Oracle Host, Oracle Port, and Oracle Service boxes.
  8. In the Database User Name box, enter the user name or schema name for the database that you are defining.
  9. In the Password box, enter the password for the associated database user name. The password must meet the criteria specified by the password policy.
  10. If you want Microsoft IIS to load and cache this database on the GE Digital APM Server to improve performance, then select the Preload Cache check box.

  11. Select .

    The data source information is saved.

Tips:

Results

Copyright © 2018 General Electric Company. All rights reserved.