Failure Rate
CDF
Reliability
Note: In GE Digital APM, there are two parameters: Mean, represented as µ, and Standard Deviation, represented as σ.
MLE
Where, is the failure time of component i, i=1,..., r or the censoring time of component i, i=r+1,..., n. If there is no censoring (complete data), r = n and the last term in the Likelihood function disappears. The terms
and
are the standard normal probability density and standard normal cumulative distribution.
Least Square
Let us denote : n = total cases, r = uncensored cases, and n - r = k = censored cases
If and
, then the parameters for
are estimated using the following equations:
In this case, and
.
Copyright © 2018 General Electric Company. All rights reserved.