Add a Logic Gate to the Logic Tree

You can add a Logic Gate node to:

You cannot add a Logic Gate node to the Failure Event node (i.e., between Failure Mode nodes). A given predecessor node can have only one Logic Gate node.

Steps

  1. Access the Logic Tree within which you want to add Logic Gates.
  2. In the upper portion of the workspace, in the Palette section, select RCA And Logic Gate or RCA Or Logic Gate, and then use the drag-and-drop method to add the Logic Gate in the design canvas to a node.

    The Properties window appears, displaying the datasheet for the selected Logic Gate.

  3. Enter the values in the following fields:
  4. Select .

    The Logic Gate is added to the Logic Tree.

Results

A link is created between:

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.