Assess the Mitigated Risk

This topic describes how to perform a mitigated risk assessment for an Instrumented Function in an SIL Analysis.

Steps

  1. Access the Recommendation that is associated with the Instrumented Function for which you want to assess the mitigated risk.
  2. Select the Mitigated Risk tab.

    The Mitigated Risk section appears, displaying the overall risk rank and the risk ranks for each risk category.

    Mitigated Risk Section

  3. Select the section that displays the risk rank.

    The Mitigated Risk Assessment window appears. The window contains a tab for each risk category configured for the Risk Matrix, which you can select to access the Risk Matrix for the category. By default, the icon appears in the cell in which the icon appears.

    Note: You cannot modify the unmitigated risk assessment in the Risk Matrix.

    Risk Matrix

  4. Select the tab corresponding to the category for which you want to assess the mitigated risk. For example, if you want to assess the mitigated risk for the Environment category, select Environment.

    The Risk Matrix for the selected category appears.

  5. On the matrix, select the cell whose value represents the mitigated risk for the selected category.

    In the cell that you selected, the icon appears.

    Risk Matrix

  6. For each category for which you want to assess the mitigated risk, repeat steps 4 and 5.
  7. In the lower-right corner of the Mitigated Risk Assessment window, select Save.

    The mitigated risk for the Instrumented Function is assessed. The Mitigated Risk section appears, displaying the overall mitigated risk rank and risk ranks for individual categories. Depending on the configuration of the Risk Matrix, the overall risk rank can be the highest or the sum of all the ranks for all the categories.

    Mitigated Risk

    Note: See the Overview of the Risk Matrix section of the documentation for additional options when working with the Risk Matrix.

Results

Copyright © 2018 General Electric Company. All rights reserved.