License Requirements
APM Connect has a three-tier license system that enables the APM Connect Framework. One of the following license types is required to take advantage of the APM Connect functionality:
APM Connect Studio
Note: APM Connect Studio contains numerous libraries that integrate with third-party products, such as GeoRaster. Questions regarding linking these libraries with GE Digital APM should be directed to a member of the GE Digital Professional Services department on an individual basis. Specific requirements of third-party products, such as additional licensing, is outside the scope of APM Connect Studio support.
Additional Licensing
The following additional licenses are required to take advantage of the SAP Adapters:
The following additional license is required to take advantage of the SAP PI Adapters:
The following additional license is required to take advantage of the Maximo Adapters:
Note: There is no additional license required to take advantage of the APM Connect Data Loader functionality.
Additional Components Required
In addition to the basic GE Digital APM system architecture, your system must also contain the following components:
Minimum Software Requirements
The third-party components listed in the following table
| Third-Party File Name | Version | Where You Can Obtain It |
|---|---|---|
| edtftpj.jar | Version: 2.0.5 | http://enterprisedt.com/products/edtftpj/ |
| ftp4j-1.5.1.jar | Version: 1.5.1 | http://www.sauronsoftware.it/projects/ftp4j/ |
| jboss-serialization.jar | Version: 1.0.3.GA | http://serialization.jboss.org/downloads |
| trove.jar | Version: 1.0.2 | http://trove4j.sourceforge.net/ |
| xom-1.2.7.jar | Version: 1.2.7 | http://www.xom.nu/ |
Recommended Software
Browser Requirements
| Web Browser | Recommended or Supported |
|---|---|
| Microsoft Internet Explorer 11 | Recommended |
| Mozilla Firefox 13 to 28 | Recommended |
| Microsoft Internet Explorer 10 | Supported |
| Apple Safari 5 to 7 | Supported |
| Google Chrome 22 to 34 | Supported |
Minimum Hardware Requirements
8 GB RAM
100 GB Free Disk
100 MB Network Interface
Recommended Hardware
I5 Processor, 2.0 + GHz
32 GB RAM
300 GB Free Disk
1 GB Network Interface
Tip: APM Connect is input and output intensive, and requires a lot of storage space. Faster storage is the best way to improve performance.
Depending on how your system is configured, these requirements may not be sufficient. Parameters that affect the hardware requirements include the number of users, modules purchased, database size, and other factors that can vary from one customer to another. For help refining your specific system requirements, contact GE Digital.
SAP System Requirements
SAP Backend System: The following versions are supported:
S/4 Hana (1511, 1610, and 1709) for the following APM Connect SAP Adapters:
Equipment Extraction
Work History Extraction
SAP PI System Requirements
SAP Backend System: The following versions are supported:
S/4 Hana (1511, 1610, and 1709) for the following APM Connect SAP Adapters:
Equipment Extraction
Work History Extraction
An SAP PO system 7.50 and later.
Maximo System Requirements
APM Connect supports Maximo versions above 7.1.1.6.
Maximo Application Server: A Maximo Application Server machine that houses the Maximo Web Services and is running version 7.1, 7.5, or 7.6.
System Architecture for EAM Adapters
Single Server Configuration (Recommended)
The single server configuration is the simplest way to configure APM Connect. However, it does include an embedded database. The following image depicts this configuration.
Note: Only one EAM system is supported for each APM tenant or database.
External Database Configuration
Many organizations choose to separate their databases. It is possible to install the intermediate repository database on an external server, and to keep the APM Connect Systems database on a different server. The following image depicts this configuration.
Note: The external configuration will affect performance. The single server configuration results in faster performance.
Deploying APM Connect
After you have installed and configured the basic GE Digital APM system architecture, you will need to perform some configuration steps specifically for APM Connect.
Supported Features in
All APM Connect features are available.
Copyright © 2018 General Electric Company. All rights reserved.