Register CIMPLICITY Plug-in with Configuration Hub
To use the CIMPLICITY plug-in, you must register CIMPLICITY with Configuration Hub after Webspace is installed.
To register CIMPLICITY with Configuration Hub. On the Configuration Hub machine, follow the steps in the Add the CIMPLICITY Node and Register the Plug-in with Configuration Hub topic.
Note: Ensure that the CIMPLICITY plug-in of the standalone server, or
relay server and all dependent servers in the Relay/Dependent scenario are registered with
the same Configuration Hub.
For more information, refer to About Registering CIMPLICITY Plug-in in Configuration
Hub.