Configure Windows Credentials
Perform the following steps on Webspace servers to set up a default Windows login on Webspace servers and avoid the need to log in every time you open a Webspace screen from a Webspace widget.
Procedure
- Open a project in CIMPLICITY Workbench as needed.
-
In the top-level folders, click and expand Computer.
-
Double-click
Configuration Hub.
The CIMPLICITY Proficy Authentication login page opens. -
Log in using ch_admin as username and your Proficy Authentication secret as
password.
Once you log in to Configuration Hub and expand the CIMPLICITY plug-in node. You will see Webspace plug-in under the CIMPLICITY plug-in node.
- Click the Webspace plug-in.
- Click General.
-
Enter Windows login user name and password in the Windows Credentials
section, and then Select Test.
For security reason, consider using a windows user that is not an Administrator. Choose a user that has permissions to run CimView.exe and access the screens directories. Refer to the latest CIMPLICITY Secure Deployment Guide for further secure setup suggestions.A success message is displayed if the credentials are valid.
- Select the Enable Webspace Strong Encryption check box to use the Webspace widget in Operations Hub.
- Click SAVE.